Home > Applications > Defense

Defense.

A military unit performs well when its equipment performs well. That's why, since World War II, U.S. military forces have depended on Cummins power.

Today's armed forces count on Cummins in 5-ton trucks, Bradley Fighting Vehicles, Multiple Launch Rocket Systems and more. From power packs and generators to material-handling equipment, from the QSB 160-hp engine to the 600-hp V903, Cummins offers a full range of power, to meet the full range of military needs. For additional information see our Cummins Diesels For Defense Brochure.

And Cummins is on the front line with support as well, with a parts and service network that is second to none. Including Fleetguard® filters and ReCon® remanufactured equipment that meets or exceeds original specifications.

Cummins military force includes:

V903 (295-600 hp)
QSC (210-300 hp)
QSB (160-230 hp)
ISM (280-450 hp)
ISL (310-400 hp)

For more information, articles and stories about the vehicles and service roles of Cummins military vehicles, plus the wider world of defense, visit the sites listed below:

United Defense
American Truck Company