Cummins Engines for European Truck and Bus

View Euro Truck & Bus Engines

With over one million Euro certified engines operating in truck, bus, coach and specialist vehicle applications around the world, Cummins brings a unique level of experience to every engine we manufacture, and the ability to provide the right engine for each installation. For vehicle manufacturers it offers a level of application expertise that few, if any, other engine companies can match. For the operator it offers world-class levels of performance. Cummins European credentials are strongly rooted, based on over 50 years of manufacturing presence and employing over 5,000 employees in the EU. OEM customers can take full advantage of Cummins application engineering support and pilot vehicle testing facility. We also draw a special strength from our huge technical and manufacturing resources in other regions. Effectively, with a Cummins Euro certified engine you get the results of a technical synergy from our most skillful designers around the globe.

As European emissions regulations are adopted around the world, Cummins engines have been developed to offer the same product enhancements, wherever they operate. Whether your requirement is for an engine to meet Euro 2, Euro 3, Euro 4, Euro 5 or Euro 6 emissions, whether you are operating in Europe, the Middle East, Africa, Russia, China, Brazil or India, there is a Cummins engine for you.

Cummins Euro 6

By using an innovative combination of the latest engine technologies, Cummins’ engines will have the capability to easily meet the Euro 6 emission standards.  Along with proven cooled exhaust gas re-circulation (EGR) and variable geometry turbocharging (VGT), the engines will also utilise our latest aftertreatment system incorporating particulate filtration (DPF) with selective catalytic reduction (SCR).

One of the most comprehensive development projects undertaken at the state-of-the- art European technical centre has completed over 80,000 hours of engine testing and more than 2 million road miles to refine and validate the technology. Leveraging our expertise, Cummins has balanced EGR and SCR technologies to reduce greenhouse gas and NOx emissions. Our solution achieves the lowest levels of fuel consumption and Adblue usage, benefiting the environment and minimising operating costs. Cummins also offers alternative fuel, low-carbon solutions with the ISLG  natural gas, spark-ignited engine.  It uses CNG, LNG or Biomethane to deliver ultra-clean, efficient power with low noise.  Along with cooled EGR and stoichiometric combustion, these engines will employ our simple maintenance-free, Three-Way Catalyst aftertreatment system to meet the Euro 6 requirements. 

For more details check out our Euro 6 website

Find a Cummins Sales or Service Location
Related Brochures

View brochures and spec sheets for Cummins engines online.

Learn More